Greetings,
According to the data sheet for the PCM1793 on page 13, it says the device automatically detects the system clock frequency. However, when I look at Table 1, 96 kHz sampling frequency at 128 fs has the same system clock frequency (12.288 MHz) as 48 kHz sampling frequency at 256 fs (12.288 MHz). How does the device differentiate between the two sampling frequencies? What do I have to do to help it distinguish between the two? Do I have to maintain a certain relationship between the bit clock (BCK) and the system clock? Page 15 mentions that the bit clock (BCK) and system clock have to be in sync, but it does specify anything further than that. By sync, do they need to be at the same frequency, 1/2, ?
Thanks,
Tobyn