Hi,
I am trying to configure PCM5142 to a sample rate of 8kHz. My system supplies the PCM5142 with an 8MHz clock at SCK input pin. The datasheet says: "SCK rates that are not common to standard audio clocks, between 1MHz and 50MHz, are only supported in software mode by configuring various PLL and clock-divider registers. This programmability allows the device to become a clock master and drive the host serial port with LRCK and BCK, from a non-audio related clock (for example, using 12MHz to generate 44.1kHz (LRCK) and 2.8224MHz (BCK) )" so every thing should be fine. But figure 26 shows that SCK can only be devided with 1,2,3,...127,128 to provide BCKO and LRCKO.
My setup:
SCK input = 8MHz
Samplerate = 8kHz
PCM5142 runs as I2S master
Frequency of LRCKO = 8kHz
Frequency of BCKO = 512kHz
Kind regards,
Niels Andersen
Elcanic A/S