Dear TI community,
I need some clarification regarding the oversampling in TAS5727 audio amplifier. We want to use TAS5727 for our module which can generate only 16 bits of data per channel but we want to be in 64fs oversampling mode. Our soc can generate serial data in 2's complement form for remaining lower LSB bits. i.e if the MSB is 1, the lower 16 bits will be 1 and if MSB is 0, it will be zero. So my question is, in 64fs and if data width from SoC is 16, is it mandatory that the lower LSB should be always 0? Can we also mention the data width in TAS5727 so that the lower 16 bits per channel are ignored ?
Your reply is much appriciated.
Thanks,
Ajith