Hello,
Is it possible to evaluate Noise suppression and AEC with PPS (Pure Path Studio) with the AIC3262-STICKEVM ?
I guess that it is possible to make a loop black from 2x MIC analog inputs thru HP output to evaluate Noise reduction, but AEC evaluation needs both Near-End and Far-End port, that is to say
Near end : 2 Inputs for 2 Mics NS, 1 x output for NE Speaker
Far end : 1 input for FE Tx path and 1 Output for FA Rx path.
My concern is that 3 inputs are mandatory, and perhpas only one is available on the AIC3262-STICKEVM.
Thanks.
Nicolas