Hi, guys,
We are using TLV320AIC32 on our board, which have pop and click problem , we are using LINE1L and LINE1R as analog input and LEFT_LOP AND RIGHT_LOP as analog output and also DOUT/WCLK/BCLK as digital ouput, 24.8 Mhz generated from cpu to MCLK is served as main clock, and sample rate is 48Khz.
I did a lot testing, it seems the pop noise is gone when it is running at 96k, which dual the sample rate, which set the register 0x07 at page 0, but we want it running under 48Khz.
I also change the ac-couple caps at INPUT side from 0.1uf to 0.47uf, it still have pop when running at 48khz,
Is anyone know what should I do to get rid of this pops, thank you!
Kevin
The register setting is following