This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Audio amp to drive 2.3ohm speaker

Other Parts Discussed in Thread: TPA2005D1, LM48312, LM48310

I need an audio amp, mono, that can drive up to 50mA into a 2.3ohm custom speaker, (115mV).
VCC will be 3.45V-3V.
Analog input will be centered at 1.25V

This is a battery powered device so it needs to be very low Iq, small space, and high efficiency.
I appreciate your suggestions.