1. For Single ended configuration, what is V peak to peak that could be fed to INP terminal with INN grounded with cap?
2.For single ended configuration what is INP DC offset of amplifier, Is it 0V or some other DC offset is there which requires the preamplifier (Audio Codec SGTL5000) line out level to be clamped at the same level of TPA2001D1 INP line.
3.Can I connect Line out of preamplifier directly with INP (Sinlge ended configuration with INN grounded) with 1 DC blocking Capacitor in series?
4.Also in datasheet at page 8, it is written that " In the typical application an input capacitor (Ci) is required to allow the amplifier to bias the input signal to the proper dc level for optimum operation " . My question : the input cap will take care of at what dc level the input signal is to be clamped or we have to take the DC level (at which the input signal is to be clamped) into consideration & calculate the value of cap. If we have to take the calculation into consideration, then please give me the algorithm for it.
5.Calculation of input capacitance requires input impedance & gain to be known. In datasheet at page : 8 it is given that " At the higher gain settings, the input impedance could increase as high as 115 kΩ. " But the table given just below of the above mentioned statement shows that with increasing of gain, the input impedance decreases, which contradicts the above highlighted statement. Please give me the correct criteria to follow for calculation of input capacitance.
6.In typical application diagram at page : 10, both Ci & Cbypass are given to be 1uF, but it is recommended to use cbypass 10 times greater than ci for pop reduction. Imagine a case in which my gain settings are such that , that Ci comes out to be 1uF, then Cbypass should be 10uF, but the range of Ci given is 0.1uF to 1uF & range of Cbypass given is 0.47uf to 1uf. So what should I do in this situation. Or what should I do typically?