Looking for suggestions on a chip amp to replace a TDA7052 BTL (bridge tied load). It's the final stage of a communications mixer which outputs to a speaker/microphone. The amp cannot be a BTL system. (The BTL arrangement of the 7052 does not allow for a common ground point in the output jack which the PTT function of the speaker mic requires). What I'm looking for is a chip amp that is not a BTL system but has similar qualities to the 7052. Preferably SOIC with a voltage controlled volume if possible. The PCB design is battery powered and has regulated +/-5V and unregulated +9V available. The current replacement plan is to use LM386M however the external parts count is high compared to the TDA7052 and space is limited.