Hi,
I'm using TPA6203A1 as audio amplifier in single ended configuration. This is my circuit
- Vdd=3.3V
- Cbypass=1uF
- Ri=22K+-1%, Rf=44K+-1%
- Ci=47nF+-10%
- R6=R7=47K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm using TPA6203A1 as audio amplifier in single ended configuration. This is my circuit
Hi, John,
Sorry for the delay in getting back to you.
What is your source doing when you're shutting down the TPA6203A1? Is it also being shutdown? Is the pop being generated by the previous stage, and being fed to our amplifier?
I noticed your Ci's are significantly smaller than Lain's, maybe increasing the value would help (this doesn't make sense, but I know his circuit works very well).
-d2