Hi! all,
When using two units of TPA3116 as a master and a slave mode,
what is the relationship of the frequency of the fOSC setting and SYNC output?
When OSC is set to 400kHz, SYNC out is 100kHz.
Is 100kHz a PWM frame frequency?
Also, according "Figure 37. Schematic" of the datasheet on Page 26, there is a low pass filter between a SYNC output and a SYNC input.
And the cutoff frequency is about 15.9kHz. It seems too low cut off frequency against the SYNC out frequency,
How is the cutoff frequency determined?
Regards,
Toshi