This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

For the PCM2900C

Other Parts Discussed in Thread: PCM2900C

For the PCM2900C, the power supply requirement is in the range of 4.35~5.25V a. When the boost converter is used to supply for this Vbus, it still outputs the voltage which is below than 4.35V. For example, 3.3~4.3V when it is disabled. What is the current leakage in this case and if the USB data line has the abnormal signals that incurs the host’s response as well?