Hello all,
i've got yesterday my pcm1863evm and, while waiting for the purepath software, i started some tests.
It is a quite complicated IC, lots of features, so my first question is:
how can i determine that, once programmed and set up, the converter is still working ?
Explanation: in case of an EMI disturbance or something, could the PCM programming get lost ? In this case how can
i sense this condition and reset/reload the ic? Writing something to a register, then polling it sometimes would be enough?
Second question: i would change all pga values at once, and i read that, setting the "linked" flag in register 5, page0, i should have
all channels tracking what is written on channel 1/left (register 1, page0).
I tried this and i wrote a gain value to register 1, page 0 (chan1/L pga level) but i see that only the left channel level is changed.
Is the "linked" flag valid only for the autogain-clipping preventing function ?
Regards
Tom