HI All,
In data sheet of the pcm1796, zero detection function is available, when i use it, it will not working properly, i try many times to detect and auto mute function when data not come. what can i do for this plz help me .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI All,
In data sheet of the pcm1796, zero detection function is available, when i use it, it will not working properly, i try many times to detect and auto mute function when data not come. what can i do for this plz help me .
Hi,
so if i am using this function (The PCM1796 has a zero-detect function. When the PCM1796 detects the zero conditions as shown in Table 2, the
PCM1796 sets ZEROL (pin 1) and ZEROR (pin 2) to HIGH.) and given condition then its working.
ZeroL & R both are connected to microcontroller and gives high signal.
this is only for 23ms and i am using it for 2-3 sec then what condition i put.