This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2005 and SKP on cable



Hi all,

I would like to use TPA2005 in bluetooth heaset as amplifier for speakers in headset.

But between amplifier and SPKs have to be minimaly 1m long cable with 4 wires. Two wires for microphone signal. Two wires for SPK:

I saw EMI filter in datasheet. Will be this filter enought for this application, or is TPA2005 inappropriate for this application?

I need some Audio amplifier between bluetooth module and SPK with small footpring and VDD between 2.9 and 4.2V. So this device looks good.

Thank you Ondrej.