Hello,
I want to convert audio data through the PCM1781 with the I2S bus, it is necessary to have the three clocks are synchronized, SCK (external oscillator: 24MHz), BCK (12 MHZ) and LRCK (192 kHz), and also DATA . I configured the liason I2S in Master mode and the PBCK clock, the problem is that I do not manage to have an analog output, my output is composed many of the different peaks like Dirac's distribution, and i can't have a correct sound like this.
Thank you for your help