This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48100-Q1 Speaker open and short circuit detection



Hello,

 

Please answer following question about LM48100-Q1

 

I need integrated speaker open/short detection function, and LM48100-Q1 has it.

But I don’t want to use I2C if possible and want to conform I can use LM48100-Q1 without I2C.

I know that speaker open and short diagnostics is only performed once after power up if I don’t use I2C.

And I want to confirm if initial register settings (for example gain etc.) are acceptable for our application, but

LM48100-Q1 datasheet doesn’t have initial (default) value after power up.

 

Please fill initial value on attached file, and advise concerns for not using I2C.

E2E_LM48100-Q1_Register.pptx

                       

Best Regards.