I've used both the TAS5706B and TAS5716 in the past with excellent results. Is one of them still the best choice today? I want audio fidelity specs equal to or better than the TAS5706B/TAS5716. Here are my other requirements:
* Minimum of 2 channels x 20 Watts (<1%THD) into 8 Ohms or 4 Ohms (I can get the speakers in either impedance)
* I2S input @ 48kHz sampling rate
* DRC
I won't be using headphone or subwoofer outputs, volume control, EQ, Pseudo-Bass.
Any suggestions?