Does the TLV320AIC26 have a built in Loudspeaker?
In the Features Section of the TLV320AIC26 it is stated that it has a "On-Chip 325-mW, 8- Speaker Driver" Does that mean that no additional loudspeaker needs to be bought , the speaker is already built in? Or does that mean that the TLV320AIC26 can drive a external loudspeaker with 325mV?
Kind Regards
Julius Gruber