I am trying to use this converter to sample a signal. I am using an fpga to drive its clocks and, looking on the analog oscilloscope the device seems to be alive but on the first 16 clock cycles I get both 1's and 0's very fast even with no input while the rest of the clock cycles I get 0's. It seems that the device is either unstable or it resets very fast. I don't understand why.
MCLK is at 8MHz and a sampling frequency of 31.25kHz. This is not a standard frequency for this IC but I don't expect this to be the cause. Any clues please?
regards,
Catalin