On pages 11 and 16, the PCM1774 datasheet mentions the RFM[1:0] bitfield in Register 81, but this register is not documented in the datasheet. Can you provide more information?
Thanks,
Bob Giaraffa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
On pages 11 and 16, the PCM1774 datasheet mentions the RFM[1:0] bitfield in Register 81, but this register is not documented in the datasheet. Can you provide more information?
Thanks,
Bob Giaraffa
There are no obvious problems; I just want to ensure that I am programming the device optimally for best performance.
I do have another question about the programming of register 84 (0x54). We are using the PCM1774 in I2S Slave Mode and are providing 24 BCK pulses per sample (i.e. 48 * fs). Our PCM1774 configuration (i.e. list of register writes) was developed by a former employee and programs register 84 to 0x02 (i.e. MSTR = 0, reserved bit 1 = 1, and BIT0 = 0). The datasheet specifies that the BIT0 default value is 1 (corresponding to 16-bit data length), and the BIT0 value of 0 is reserved.
I don't have any supporting documentation to know if writing register 84 to 0x02 instead of 0x01 was previously recommended by TI, or just a mistake. Would there be any reason to set register 84 to 0x02?
Thanks,
Bob Giaraffa