Hi,
I am planning to use only one input and grounding the other. Grounding one input would result to its associated driver being off. Does that mean that I can leave said associated output pins floating? Specifically, pins 37 to 48? Or are there other things I would need to do for said pins?
Also, I added an LC filter in Figure 40 to the LOUT+/LOUT- of the TPA3004D2EVM and found an unwanted DC voltage of ~6.68V across the load. I’d like to get rid of said voltage by adding capacitors shown in Figure 40A. However, I’m having a difficult time calculating what value capacitor I need. How do I go about finding the capacitor value I need that will keep the range of 20Hz to 20KHz at the line out? Is there another way to get rid of the DC voltage?
Please advise.
Thanks!