Hi folks,
In TAS5760LD datasheet, there are two THD+N vs Output Power graph in the same condition.
For example Figure 5 and Figure 6 in page 14, as below picture:
What's the difference between them?
or it's typo of PVDD? compare to TAS5760MD, the PVDD might be 18V?
The same questions at Figure 18 & 19( p17)., Figure 28 & 29(p19), Figure 35 & 36( p20).
Thanks.
Regards,
Will