Hi TI,
I was wondering if it is possible for the TAS5727M to reliably drive a transducer with 2.3 ohms RL (including cable series resistance), in PBTL mode, PVDD = 18V. The TASW5727 datasheet indicates a RL (PBTL) minimum of 2 ohms. We would like to drive our transducer to fairly high output levels, and would like to know what the power limits of the TAS5727 are when driving a 2 ohm load.
Our output filter is L = 15uH, C = 680nF.
We have tried this in the lab, and it appears to work. But we are concerned about long term reliability and risk of damaging the amplifier. It is possible we could add a small heatsink if necessary.
thanks in advance for your help / comments..
best,
Andrew Kimpel