This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254 EVM how to settting 192K I2S input in master mode



Hi Sir,

AIC3254 EVM how to settting 192K I2S input in master mode

  • Hi,

    Please take a look at the following script. It is an example of how to configure the codec for a 192ksps in master mode:

    ##############################################
    # High Performance Stereo Recording
    # ---------------------------------------------
    # PowerTune mode PTM_R4 is used for high
    # performance 16-bit audio. 
    #
    # For normal USB Audio, no hardware change
    # is required.
    #
    # If using an external interface, SW2.4 and
    # SW2.5 of the USB-ModEVM must be set to
    # HI and clocks can be connected to J14 of
    # the USB-ModEVM.
    #
    # IN1L/R is routed to the LADC/RADC in a
    # single-ended manner.
    ###############################################
    
    
    
    ###############################################
    # Software Reset
    ###############################################
    #
    # Select Page 0
    w 30 00 00
    #
    # Initialize the device through software reset
    w 30 01 01
    #
    ###############################################
    
    
    
    ###############################################
    # Clock Settings
    # ---------------------------------------------
    # The codec receives: MCLK = 11.2896 MHz
    # BLCK = 6.144 MHz, WCLK = 192 kHz
    ###############################################
    #
    # Clock configuration
    w 30 00 00
    w 30 04 03
    w 30 05 12
    w 30 06 28
    w 30 05 F2
    w 30 12 87
    w 30 13 83
    w 30 14 20
    w 30 1D 03
    w 30 1E 81
    w 30 1B 0C
    w 30 21 10
    #
    ###############################################
    
    
    
    ###############################################
    # Signal Processing Settings
    ###############################################
    #
    # Select Page 0
    w 30 00 00
    #
    # Set the ADC Mode to PRB_P1
    w 30 3d 0d
    #
    ###############################################
    
    
    
    ###############################################
    # Initialize Codec
    ###############################################
    #
    # Select Page 1
    w 30 00 01
    #
    # Disable weak AVDD in presence of external
    # AVDD supply
    w 30 01 08
    #
    # Enable Master Analog Power Control
    w 30 02 00
    #
    # Select ADC PTM_R4
    w 30 3d 00
    #
    # Set the input powerup time to 3.1ms (for ADC)
    w 30 47 32
    #
    # Set the REF charging time to 40ms
    w 30 7b 01
    #
    ###############################################
    
    
    
    ###############################################
    # Recording Setup
    ###############################################
    #
    # Select Page 1
    w 30 00 01
    #
    # Route IN1L to LEFT_P with 20K input impedance
    w 30 34 80
    #
    # Route Common Mode to LEFT_M with impedance of 20K
    w 30 36 80
    #
    # Route IN1R to RIGHT_P with input impedance of 20K
    w 30 37 80
    #
    # Route Common Mode to RIGHT_M with impedance of 20K
    w 30 39 80
    #
    # Unmute Left MICPGA, Gain selection of 6dB to make channel gain 0dB
    # Register of 6dB with input impedance of 20K => Channel Gain of 0dB
    w 30 3b 0c
    #
    # Unmute Right MICPGA, Gain selection of 6dB to make channel gain 0dB
    # Register of 6dB with input impedance of 20K => Channel Gain of 0dB
    w 30 3c 0c
    #
    # Select Page 0
    w 30 00 00
    #
    # Power up LADC/RADC
    w 30 51 c0
    #
    # Unmute LADC/RADC
    w 30 52 00
    #
    ###############################################
    

    The USB I2S switch (SW2 on MODEVM-INTERFACE BOARD) must be disabled in order to use the codec in master mode.

    Best regards,
    Luis Fernando Rodríguez S.

  • Hi Sir,

    Thanks

    If we use 24Bit, only setting P0 R27 B5-4, right?

  • Hi,

    You're right. P0 / R27 / B5-4 must be configured as "10" to use 24-bits.

    Best regards,
    Luis Fernando Rodríguez S.
  • Dear Sir,

    If we want to analog in/out with EQ setting, we also need provide MCLK/BCLK/LRCLK? or MCLK only?

  • Hi, iehncent,

    It can be both configurations. If the codec is configured in master mode, it would be required only the MCLK. If it is configured in slave mode, MCLK, BCLK and LRCLK would be required.

    Best regards,
    Luis Fernando Rodríguez S.