Other Parts Discussed in Thread: SRC4392, DSD1794A
Hi
With your support i finally led in the use of SRC4392 with two DSD1794A configured in monaural mode. I resulted in the DSD1794A because provides separate inputs for DSD and PCM data. I should remember you that will include in my project a USB2.0-Audio module that provides DSD and PCM data. Till now everything is going very well in the schematic drawing of project. Today, by looking in the DSD1794A datasheet the suggested analog low-pass filter for the output of DAC i got stuck again! The reason is that for PCM converted data the suggested filter (page 33) has a Fc=162KHz whilst for DSD converted data the filter (page 34) is totally different with Fc=38KHz.
I know that the out of band noise in DSD format, starts from lower frequency while in PCM format starts from a higher frequency.
My question is what i can do now? If i will implement the DSD suggested output filter with Fc=38KHz by sure will have a perfect response in DSD audio files, in the cost of strangling the high frequencies of PCM audio files? If i will implement the PCM output filter with Fc=162KHz then will have perfect response in PCM audio files but a lot of noise when DSD files will be converted?
Or if i will implement the DSD output filter the impact of Fc=38KHz on the high frequencies of PCM audio files will be negligible and so there is no reason to fear so much?
Or the inverse? I mean that the high frequency noise of DSD audio files will be negligible in the case of PCM output filter with Fc=162KHz?
What they do other constructors for this issue? Do they build special antialiasing filters suitable for both DSD and PCM audio files? Or they simply disregard the issue of PCM straggling by using the lower cut-off (38KHz) DSD filter having as priority the elimination of any noise?
I came accross the internet for two days but i couldn't find anything about this issue.
Have you any experience on this issue? Is there a compromising output low pass filter with a cut off frequency which could satisfy the requirements of both DSD and PCM audio files? And this filter is different from those you present in DSD1794A datasheet?
Any help will be welcomed!
Thanks
Regards
Fotis