Hi,
I have an audio system where we are using a DRV135 and upto thirteen INA134 receivers over a twisted pair unshielded cable. the bus length is about 400meters with a receiver placed every 30 odd meters. Is this a suitable topology for DRV135 to driver?
My logic is the input impedance of INA device is 50k-ohm while the DRV can swing upto 85ma into a line impedance down to 600ohm. So effectively there is sufficient head room.
We are having a bit of problem, with amplification level falling through out the bus in field. the problem was never faced in lab.
Any one with working knowledge of these devices who can help?