Dear Sirs,
My customer asked to me below question.
They use a combination of the PCM9211 and TAS5558.
PCM9211 can be selected of MCLK at the time of SPDIF input is 128fs, 256fs, only the selection of 512fs.
TAS5558 has switched the MCLK at 88.2 / 96kHz with ASRC (actually SRC) behavior.
So if the input of the TAS5558 is fs = 32kHz, no sound because it does not become an integer multiple.
Please tell me how to set the case of input 32kHz.
Best Regards,
Y.Hasebe