As TAS5162 and similar amplifiers are meant for audio applications, the upper operating switching rate is specified to be 432kHz in the datasheet.
We are trying to use the above chip to amplify a PWM signal of 1.2Mhz and I see that the output is quite satisfying. The target energy to be delivered will be under 5-10Watts and the PVDD supply only 20V (the IC is rated for 2x210Watts and 50V).
So we would like to ask if have you tested the amp for higher frequencies. Is heating the only reason of the 432kHz limit or is there some other failure/degradation mechanism to be expected?
Thank you for your support