Hi
i am trying to build power amplifier whose output should be 10-20w to drive the 8 ohms speaker for our active noise control system.
honestly the optimal solution is to find a mono power amplifier IC to do that. but i cant find a mono which satisfy the output power requirement of our speaker.
since i need only output one channel signal, i am just wondering if the following configuration is feasible:
1. for SE mode, only use one channel and one speaker and leave alone another.
2. for BTL mode, ground one input end and connect signal to another (i'm not sure if the distortion will appear using it this way and i noticed i need a DC blocking caps at the output cos dc wouldnt be cancelled)
any suggestion will be appreciated.
Jensen