Hi
TPA5050 has input/output buffer but we can not see how much buffer is used in operation.
1. Is there reset command to clear them? If no, how to clear them?
2. Do you have more detailed block diagram?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPA5050 has input/output buffer but we can not see how much buffer is used in operation.
1. Is there reset command to clear them? If no, how to clear them?
2. Do you have more detailed block diagram?
BestRegards
Hi Luis
Thank you for your reply.
1. If power off reset is done, are there recommended power on / off sequence?
2. TPA5050 has buffer (shift register) for delaying data and we are assuming these registers have their own reset terminal.
What is the condition of the buffer when the power off reset is done?
3. How long should we take for power off/on reset to clear these registers?
There is following description on the datasheet.
>BCLK is the serial audio bit clock, and it is used to clock the serial data present on DATA into the serial shift register of the audio interface.
If BCLK is not supplied (stopped), the data buffer for delaying would not be updated. When BCLK is supplied again, previous buffered data would be garbage that is not needed. So, we must clear these buffer properly.
BestRegards
Hi Luis
Thanks for your reply.
We can refer the default state of the control registers(0x01-0x08) but not buffer.
What is the default state of the IO buffer and Delay memory?
When the power off reset is done, the buffer all cleared with "0"?
And we want PoR sequence, could you please show us?
Thank you for your help.
BestRegards