Hi
If we write 1 to complete Update register, how to back to 0?
After required delay accomplished, this register becomes 0 automatically?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, na,
1. Effectively, once '1' is written in bit D0 of register 0x08, the mute is applied as described in Complete Update Register (0x08) section of datasheet.
2. Please ensure that the mute is end to write '0' in this register. If '0' is written before mute ends, the operation could be interrupted.
3. Yes, there's no problem. This register can be written individually with single byte write.
Best regards,
Luis Fernando Rodríguez S.