Hi Team,
The customer has the issues about TPA6112A2. He wants to control the device mute through the SHUTDOWN pin.
The requirements are as follows:
First,the device must be mute at once when the SHUTDOWN pin is high level.
Second,after 3~5 seconds, the SHUTDOWN pin is low level and the device should work normally.
Can the SHUTDOWN pin of TPA6112A2 meet the customer's requirements? If not, please recommend me a suitable IC.
Thanks.
Best Regards,