Hello!
What could be the reason for the fact, that TLV320AIC33 in Master mode sometimes ( approximately 1-2 out of 10 switch-ons of device in which it is onboard ) produces BCLK with Duty cycle ~ 37% / 63 % instead of nominal 50% / 50% ?
This behaviour causes malfunction of downstream devices.
PLL is enabled and D=0000. MCLK = 18,432 MHz, WCLK = 48 kHz, BCLK = 3,072 MHz, R=1, P=3, K=J=16.
I understand, that its difficult to give an exact reason for such a behaviour, but please give me a hint!