Dear Sirs at TI,
I've made a prototype RIAA Phono pre amplifier with LM4562. The unit is fed by regulated power supply using 7815 and 7915 IC's. To avoid oscillations during testing, the input has been shorted to Gnd. Each rail is consuming 10mA at 15Vcc.
I am surprised that the case of the IC is very warm to the touch, it reached 45°C (circa 113°F). Is this the actual temperature of the 4562 when powered on?
I look forward to hear from you soon.
Kindest Regards,
Enrico Borsetti