This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1864evm 4 Channel TDM Mode shows one channel over USB

Other Parts Discussed in Thread: PCM1864EVM, PCM1864

TI,

I have a setup where the PCM1864evm has 4 channel microphone in.  When I set up the EVM with the included USB-I2X cable to connect to the computer, I see one device.  

The PCM1864 is sending data in TDM mode, 64-bit, 16bit-per-channel, over four channels.

How can I view each channel individually on the computer? Do I need to hook it up some other way than the USB-I2X adapter board?

Regards,

Aaron Jones