This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

New audio amplifier design request

Other Parts Discussed in Thread: TLV342, TPA321

Hi TI,

Can I request from you to develop a new ULP device the same as TPA321, but using TLV342 operational amplifiers?

My draft results was quite good with 32 Ohm load.

So I expect such benefits:

- ultra low power peak output less than 130mA (20kHz bandwidth);

- ultra low power supply current - less than 400 uA (would be nice to lower this parameter even further, each TIA consumes only 70 uA).

- ultra low shutdown current - less than 0.01 uA;

- unity-gain bandwidth -  2.2 MHz.

By the way, I like the performance of both such devices, but power consumption is a crucial factor.

I hope you'll find some benefits to have this unit in your portfolio too.

Thanks,

Alexey