Hi, I'm troubleshooting a commercial PA system which uses a TAS5261, The TAS5261 is failing short, the replacement board only lasted a few months, could this be due to failing lead acid batteries? or current or voltage peaking in the output filter? The inductors are 10uH Bypass caps 1.0uF the speaker is 4 ohm.
Initially the system worked ok for ~3years, when the amp board was replaced the batteries were not considered and thought to be ok but after the second board failure one 12v battery was found to have failed. could this be an under volt problem?
David