Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4190: Questions of the SRC4190's RCKI and SDOUT

Part Number: SRC4190

Hi Sirs,

We have two SRC4190's questions need to consult with product line:

1. Customer's Codec has no MCLK output. Can we use a discrete 12.288MHz or 24.576MHz oscillator to send RCKI signal to the SRC4190?
2. If we program the SRC4190 to slave mode at input, master mode at output. Will output pins become Hi-Z or logic low in reset mode?

Thank you and Best regards,

Wayne Chen
01/04/2017