This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1865EVM: PCM1865 EVM Mode2 4 ch usb stream

Part Number: PCM1865EVM
Other Parts Discussed in Thread: PCM1865

Hello,

Following instructions from : https://e2e.ti.com/support/data_converters/audio_converters/w/design_notes/2790.how-to-revive-a-usb-audio-evm

I was able to configure the USB-AudioEVM driver to support multiple sampling rates.

However, I wish to use the PCM1865 for it's 4 ch potential.

Is there a driver image that can be downloaded on the USB-I2X board which grants the PC access to 4 ch recordings?

I.E  is it possible to receive 4 ch data: ch1[L], ch1[R], ch2[L], ch2[R] through the USB-I2X?

Thank you

  • Hello, Matias,

    Welcome to E2E, Thanks for your interest in our products!.

    Unfortunately, we only have firmware available for two channel operation. 

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Thank you Diego,

    For Mode2, does the PCM1865/PCM9211PT (Slave) provide two I2S outputs, for Ch1 & Ch2?

    Is the USB-I2X controller (master) limiting to 2 ch operation?

    May the PCM1865 (slave) be connected to a different master board, and route two I2S[L][R] from CH1[L][R] and CH2[L][R]?

    Thanks