Hi,
I would like to use 12KHz sampling rate(WCLK) on the PMC5100.
Below is my question,
What SCK frequency should I use for the 12KHz sampling frequency?
below capture has in data sheet page24 but it does not have 12KHz sampling rate information.
Question1. so, how to using the system clock frequency value?(ex. example or reference guide)
Qustion2. If i use for 12KHz sampling rate can i use quard divide of the 48KHz sampling rate base?
ex) - SCK : 1.536MHz(quard divide of 48KHz) or
- BCK : 384KHz(for 32Fs)
- LRCK : 12KHz
Regards
YK Jung