This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760LD: DAC type

Part Number: TAS5760LD

Hi, I was just wondering what type of DAC is used in this chip (TAS5760).to convert the I2S data sample to PWM samples.
Does it have a particular name?

-Erblin

  • Hi, Erblin,

    We can't provide details about the internal architecture of the TAS5760LD, what we can say is that the data from the I²S input goes through a DAC stage and then to an analog modulator that uses traditional comparison of analog signals to create the PWM required for the power stage.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer