Hi, I am using TLV 320 DAC 3120.
Please tell me how to properly shut down the DAC channel.
Below is my processing order.
I referred to the description of 5.7 CLOCK Generation and PLL in the data sheet.
1.Drop the D7 bit of Page 0, Register 63.
2.Polls until the D7 bit of Page 0, Register 37 is dropped.
3.When the D7 bit of Page 0, Register 37 goes down, power down in order of MDAC and NDAC.
However, since the D7 bit of Page 0 Register 37 will not drop, it will continue to poll.
Incidentally, there is a description that the power status flag of D7 bit and D3 bit of Page 0 Register 37 should be read in the document of TLV 320 DAC 3120, but the D 3 bit is a reserved area, is not it?
By the way, I do not use PLL_CLK.
best regards
Taku Imaizumi