I'm working on Amplifier design by using TPA3112D1.
To get reference test result, I measured THD, Frequency response, S/N rate etc by using TPA3112D1EVM.
But the frequency response is going down to less than '-1dB' at over Approx. 3.4kHz.(refer to below graph)
* Test conditions
-Input voltage : DC24V
-Input audio signal: 0dBm(Unbalance)
-PLIMIT: Max
-Gain setting: 20dB(All jumpers are inserted on EVM)
-Output(Load): 8ohm resistor via matching transformer(8ohm : 8ohm)
-Measuring point: 8ohm resistor
-Test equipment : APX515(Output impedance: 600 ohm / Input impedance: 100 kilo ohm)
-dBrA: Output level at 1kHz
Is there any special method for the test?? or Is my way to measure wrong?