This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I have configured the TPA3244EVM for PBTL connected to an 4Ω load. The datasheet specifies that the amplifier has an inverting voltage gain of 20dB (10V/V). But I measure a larger gain, approximately 15.9 V/V. For example with the AP2722 I source a 500mVrms input at 1kHz and measure 7.95Vrms on the output. Am I missing something? Do the line in buffers gain the inputs as well?
Thanks!
Paul
Hello Paul,
The buffers are preset for a gain of 1. I will need a little more information on your system set up. Are you using single-ended or differential input? Also are you sending a sine wave input signal?
Thanks,
Robert
Hi Robert,
Using a single ended input, I see the following:
C2 is my SE Input signal. C3 is the A/C output of the TPA3244EVM and C4 is the B/D output, both referenced to GND. The math waveform is the difference between C3 and C4. The scope is measuring a 100mVrms input and 1.57 Vrms output, approximately 15.7V/V gain.
For differential inputs, I see that the can seems to be about 8V/V:
This time, C1 is INB, C2 is INA, C3 is A/C, and C4 is B/D.
Below is the AP configuration for the differential configuration.
Please let me know if there is more information you need.
Thanks!
Paul
Ok, I understand why SE input has 2x the gain of the differential input.
Looking at the schematic, we can see that the RCA input A is buffered and inverted for INA, Then if J4 is set to SE, the same signal is buffered and inverted again for INB. So this means that the actual differential inputs of the TPA3244 is seeing 2x the input amplitude of the original signal from the AP. When if differential mode this circuit does not change the magnitude of the input.
But this still leaves me wondering why the TPA3244 circuit has a gain of approx 8X rather than 10X, is there some kind of attenuation with the output filter/LC?
Thanks!
Hi Paul,
I have to apologize. I misunderstood your initial question regarding the op amps. Yes you are correct, though the op amps are set to unity gain, if the signal is single-ended then the signal does get X2 to create a differential signal.
I have also run the test using the information you provided and was able to recreate your results. There does appear to be a gain closer to 8X. Your assessment on it being the LC filter is the most likely cause of a majority of the loss seen.
Regards,
Robert
Hi Paul,
I did more research into the TPA3244 gain and found out that the datasheet has an error in it. You should only get 18dB gain out of the TPA3244 instead of 20dB as seen in the datasheet. Thank you for helping me find this and we will be correcting this mistake shortly.
Best Regards,
Robert