Other Parts Discussed in Thread: TAS6424,
Hi,
I was trying to remove J12 and add to the J12's pin, which is the VBat 12V, and to the main PVDD I connected 24V
GND was common.
I was not able to start the EVM board like this, because the FAULT led is on.
Going back to 12V supply and J12 on, it works.
Is there a special workaround to use the EVM board from more than 18V?
Thanks,
Tamas