Other Parts Discussed in Thread: LM4865, TAS2521, TAS2505
Hi,
I have designed pre-amplifier for a sound system, now the output from the pre-amplifier will be connected to amplifier to increase the power so that it can be connected to 500mW speaker, with volume control. I am thinking of using LM4995, but there is no separate volume controller, is it possible to change the feedback resistor using pot as a variable resistor to change the output volume.
I have one more question, is it possible to connect speaker and headphone jack in parallel, as to allow sound to come in both headphone and speaker at same time. I have already read about LM4865, (it has separate volume control function). In LM4865 headphone detect function will disable the main speaker, whenever it will detect the 3.5mm jack, which we don't require. Even after insertion of headphone jack, output should come in both main speaker as well as in headphone also.
Could you please help in proper selection of audio amplifier, Vmin of amplifier should be at least 3.3V.
Regards,
Tapas