This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1803A: Connection processing of logic pins for PCM1803A

Part Number: PCM1803A

Dear Sirs,

My customer asked us about connection processing of logic pins for PCM1803A.

Is a pull-up resistor and pull-down resistor necessary at LOW / HIGH on the Logic pin shown below?
PIN 8, 16, 17, 18, 19, 20
After checking the datasheet, these input pins were Schmitt trigger inputs.
Also it was pulled down internally by 50 kΩ.
For this reason, I think that it is necessary to fix both the pull-up resistor and the switch as necessary, and to fix the pull-down resistor and to use the switch.
Is this correct?

Best Regards,

Y.Hasebe