This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TLV320AIC3268: Audio serial interface

Part Number: TLV320AIC3268

Tool/software: Linux

Hi Ti,

I am using AIC3268 in our custom board.

There are 3 audio sources:

1. Analog line in signal

2. Digital HDMI audio

3. Digital SDI audio

As I know, there are 3 audio serial interfaces in AIC3268.

Is it possible to clock out the following I2Ss to our main chip?

1. I2S with mixed audio (line in + HDMI +SDI)

2. I2S with HDMI audio

3. I2S with SDI audio

I could mix line in, HDMI, SDI audio in miniDSP and clock out mixed data in ASI1 to our main chip already.

If I want to clock out HDMI audio in ASI2, such as:

HDMI audio->SRC(sample rate converter)->AIC3268 ASI2 in->AIC3268 ASI2 out->main chip audio serial interface.

The BCLK and WCLK of ASI2 both connected with SRC and main chip. The clock mode is master mode. is it OK?

Thanks

BR,

Steven