This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760M: A function difference between TAS5760M and TAS5760L

Part Number: TAS5760M
Other Parts Discussed in Thread: TAS5760L

Hello support team,

 

The customer want to eliminate the MCLK input for TAS5760M but only for TAS570L d/s says below:

The TAS5760L device supports SCLK to LRCK ratios of 32, 48, and 64. If SCLK is running at 64 × LRCK, MCLK can be tied directly to SCLK. Otherwise, MCLK must be driven externally.

 

Of course, the customer SCLK is running at 64 × LRCK. Even so TAS5760M can’t be tied directly to SCLK? Or TAS5760Mcan use?

 

Best regards,

Izumi Maruyama