This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4871: high frequency output

Part Number: LM4871

Hello team,

My customer got a 3.4MHz 0.9Vp-p sinusoid waveform from pin8 to GND even no audio input, we can still see this high-frequency signal with audio input.

Could you help advise how to solve this issue?

Dongbao

  • Hi Dongbao,

    Perhaps this is a noise signal that is coupling into the device output. In that case you could add a ferrite bead filter at the output.
    One question: Why is there a cap between Vo1 and Vo2?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low power Audio & Actuators
  • Hi Ivan,

    Thanks for your reply.
    Customer test this device with clean 5V input, and other parts were not working during test. Another comment is we can see the signal from pin 4 to GND when C104 is removed. Any other comments regarding the possible root cause?
    I think the cap between Vo1 and Vo2 is used for filtering.

    Dongbao
  • Dongbao,

    Have you tried by removing C133? And perhaps also C135 and C136?
    I'll keep looking for possible root cause.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low power Audio & Actuators
  • HI Ivan,
    Thanks for your reply. We can solve this problem by reducing c135/6 from 2.2nF to 100pf, Could u let me know the reason? i didn't see very long route of the output.
    Dongbao
  • Dongbao,

    Capacitive loads could drive the Class-AB amplifiers into instability. Perhaps this is what is happening here.
    If C135 and C136 are needed they could try to add series resistors at the outputs (pins 5 and 8) to isolate the capacitance from the device outputs.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low power Audio & Actuators